Key Takeaways:
- Standards like UL 2416, NEMA, and GR-63-CORE guide product safety and reliability.
- Regulatory compliance ensures long-term protection against electrical, environmental, and structural stress.
- Great Lakes designs and tests enclosures to meet the standards that matter most.
Every data environment faces its own kind of stress. It might be the steady vibration from nearby equipment, a sudden power fluctuation, or years of exposure to dust, humidity, and heat. In each case, a rack or cabinet has to do more than hold equipment, it has to protect it.
That protection starts long before installation. It begins with the standards behind the design — UL tests for electrical safety, NEMA ratings for environmental protection, and GR-63 requirements for structural stability, among others.
Together, these standards define how well an enclosure performs when conditions aren’t ideal, which, in most facilities, is most of the time.
Standards Are Engineering, Not Red Tape
At first glance, standards may look like technical checkboxes. In reality, they represent decades of engineering research and testing designed to prevent failure. Each standard addresses a specific type of risk, helping to ensure that enclosures perform consistently and safely across industries.
While there are many standards that guide rack and cabinet design, the following are among the most common and most widely referenced in the U.S. market.
Examples of Key Standards
UL2416
The UL 2416 standard covers rack and cabinet systems for information and communication technology (ICT) equipment. It evaluates how enclosures manage electrical safety, load capacity, and fire prevention.
A UL-listed cabinet helps ensure proper grounding, stable weight distribution, and materials that resist heat and flame spread.
For facilities managers and inspectors, a UL 2416 listing is an immediate indicator that the product meets recognized safety and performance criteria.
NEMA
In industrial environments, airborne particles, vibration, and moisture are constant challenges. NEMA ratings define various levels of enclosure protection against these environmental factors, helping ensure equipment reliability.
For example, Cabinets rated for NEMA 12 are often used in manufacturing, utility, and mechanical spaces where contaminants could compromise electronics.
Choosing an enclosure with an appropriate NEMA rating extends equipment life and reduces maintenance caused by environmental exposure.
GR-63-CORE
Developed by Bellcore (now Telcordia), GR-63-CORE sets standards for the physical robustness of network and data center equipment under vibration and seismic stress.
Testing simulates multi-axis ground motion while the cabinet is fully loaded, ensuring it remains upright and functional.
For facilities in seismic or high-vibration regions, GR-63-CORE compliance provides a higher level of assurance for uptime and safety.
Why These Standards Matter
Modern IT equipment is denser, heavier, and hotter than ever before.
Standards like UL 2416, NEMA, and GR-63-CORE — along with many others used across the industry — ensure that enclosures are built to handle real-world conditions: electrical safety, environmental durability, and structural resilience.
For projects funded under U.S. infrastructure initiatives, these certifications also align with Build America, Buy America (BABA) requirements, which prioritize domestic manufacturing and compliance for federally supported infrastructure project.
Built to Standards. Built to Survive.
At Great Lakes Data Racks & Cabinets, standards are part of the design process from the start.
Every cabinet and enclosure is engineered, tested, and documented to meet the requirements that matter most for safety, reliability, and long-term performance.
Because the best time to think about compliance is before the dust, heat, or time itself test the limits of your infrastructure.
Learn more about our UL-listed, NEMA-rated, and seismic-certified enclosures at greatcabinets.com.